HomeSUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
System ProductsNotificationsProduct DocumentationKnowledge BaseService PartsNewslettersSupport HelpSecurity & Other Updates
Home > SUPPORT > Security & Other Updates > Microsoft Non-Security Updates > Updates
Enter search criteria within   > Advanced Search
Products Major Release Status
Page of
< Previous | Next > 
Title (Active Link)DescriptionDate CreatedMajor ReleaseStatusProducts 
Microsoft Non-Security KB971265 This patch resolves when a memory leak issue in the Lsass.exe process causes an application or a service to stop responding if the application or the service uses the NTLM authentication on a computer that is running WindowsServer 2K8 or Vista.9/12/2011InstallTesting CompleteExperion
Experion TPS
Microsoft Non-Security KB933239 This patch is resolved a problem of Console Stations (Windows XP SP3) is inability to connect to the Cluster Server if the Domain Controller is off line.12/10/2009InstallTesting CompleteExperion
Experion TPS

< Previous | Next >