HomeSUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
OverviewProject Engineering and ConsultingTrainingMaintenance and SupportOptimization ServicesIndustrial SecuritySystem MigrationServices A-Z
Bailey
Fisher
Foxboro
Honeywell - QCS
Honeywell - TDC 2000 Data Hiway
>BASIC Controller
>BOS/EOS
-Features
-Why Buy
-FAQs
-User Benefits by Role
-Manuals
>DHP
>Extended Controller
>GPCI
>Hiway Care Program
>Multi-function
>PCSI
>PIU
Honeywell - TPS/TDC 3000
Moore
Rockwell
Rosemount
Siemens
Yokogawa
Honeywell - QCS1
Home > SERVICES > System Migration > Honeywell - TDC 2000 Data Hiway > BOS/EOS > FAQs
 

BOS/EOS: Frequently Asked Questions

Q: What are the benefits of migrating a BOS/EOS solution to Experion?
A: With intensifying governmental requirements and increasing competition, many customers have been requesting additional functionality to be provided on non-LCN-based Data Hiway systems. Operators need a better view of the process and the business aspects of running the process. Experion meets these requirements and more by providing:

  • Improved connectivity to multiple subsystems.
  • Data/event archiving, as well as long-term storage of process data and operator actions.
  • Enhanced alarming and alarm management tools.
  • Enhanced trending and archival playback with zooming and scrolling.
  • Improved process graphics with conformance to ASM Consortium guidelines.
  • Plant network connectivity:
    • Data Hiway information to spreadsheets and other documents, and data export via ODBC/OPC, etc.
    • Rapid report format/content changes and an integral reporting package.
  • Operators are provided more information from:
    • Higher-level systems
    • Variety of subsystems
  • Shift supervisors/engineering have remote view of the process, and can dial in from office or home.

Additionally, Experion is based on an open architecture with a high degree of networking and data base access capability. This capability, in conjunction with support of existing Data Hiway devices, provides for rapid payback to the customer.

Q: What if the user employs several Enhanced Operator Stations as the primary operator interface? Will he still have multiple databases to maintain after migrating to Experion?
A: The database management problems of the past are no longer an issue. Experion provides one, easy to manage database for all data types.

Q: Does Experion provide trending comparable to the existing BOS/EOS trending?
A: Experion trending goes far beyond the limits of BOS/EOS trending and provides useful history information to the operator for analyzing and controlling the process. All trend data is presented to the operator with the capability to zoom, pan and select specific trend data in real time. Data points to be trended can also be selected and grouped together “on the fly” to facilitate real-time process analysis.

Q: What is the user needs to improve/automate his reporting to meet new requirements? Will the migration to Experion be helpful?
A: In addition to providing a larger number and type of reports, Experion enables reports to be electronically transmitted via the plant network to all interested parties. No longer will you need to have an operator or engineer manually read the printed reports, perform additional calculations, and then create new reports that get passed along. Additionally, all data can be automatically populated to an Excel spreadsheet so that data manipulation, analysis and distribution can be automated.

Q: What kinds of totally new control capabilities will be available after migration to Experion?
A: Experion provides a host of improved control functionalities, including model-based controls and an integrated loop and logic capability for improved process constraint control. Cross-unit controls are implemented in easy to use software versus the hard wiring between controllers that was required in the past.

Q: What if the user wants to simply “copy” existing control schemes over to Experion without making any changes? Is there a means to do this?
A: Control Match services can simply duplicate the controls that were running in your existing system into Experion. All point types and standard algorithms of the BOS/EOS can be easily migrated.

Q: How quickly can the physical migration to new controllers occur at the plant/mill site?
A: The time typically required for physical migration is 2 to 4 hours. Much less time is needed if you are migrating a small system. There are two reasons for the short downtime: one, the migration kit is a plug-and-play design (just disconnect cables, remove a few screws per assembly, install new assemblies, and connect or reconnect cables); and two, I/O checkout can be quite efficient (all of the existing I/O and cables were operational and correct before the migration, and the new cables and assemblies are tested and verified in the factory before shipment). 

Q: In a case where the user has limited free floor space, will additional cabinet space be needed for the new Experion controllers?
A: In most cases, the new control system can be mounted into the existing TDC 2000 cabinets. No additional floor space may be needed.

Q: Are calibration and test points available on the migration kits for on going maintenance?
A: Yes, calibration and test points are provided.

Q: Do the migration kits have any active components, such as CPUs, networking, etc.?
A: No, all Signal Match migration hardware is created using passive components. This greatly increases reliability and longevity, and reduces the number of possible fault paths.

Log In
Search

  Advanced Search
Contact Us
Contact Honeywell Process Solutions