Q: Why is ‘forming the sheet’ the most important step in papermaking?A: Stock distribution at the wet end sets the stage for every step that follows, from pressing through drying, coating and calendering. Mechanical issues with the headbox often restrict proper formation and induce uncontrollable profile variations.
Q: What is the ‘apron’ and what part does it play in the overall process?A: The headbox frontal area is called the apron (lower lip). The importance of the apron can be seen from the following facts:
Q: What are the ways to achieve apron improvement?A: There are two means of apron improvement:
Mechanical Stress uses force (brass plates, clamps and lead mallets) in order to reduce variation "peaks." This method only re-distributes the variation over a wider area, but does not eliminate the problem. It is considered a short-term solution.
The proven and best method used by Honeywell is Thermal Improvement, employing a combination of heat and cold water. Thermally improved aprons tend to retain their shape so the degree of variation reduction is significantly higher.