HomeSUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
OverviewAsset ApplicationsBusiness ApplicationsControl ApplicationsOperations ApplicationsInstrumentationMachine Control & SafetyControl & Safety SystemsWirelessTerminal Automation ProductsProducts A-Z
Alarm Management
Blending & Movement Automation
Emissions Monitoring
Information Management
Operations Management
Planning and Scheduling
>BLEND
>ASSAY2
-Features
-Why Buy
-FAQs
-User Benefits by Role
-Literature
>Production Scheduler
>RPMS
>SAND
Production Management
Simulation
Home > PRODUCTS > Operations Applications > Planning and Scheduling > ASSAY2 > FAQs
 

ASSAY2: Frequently Asked Questions

Q: What is ASSAY2?
A: ASSAY2 is a crude oil evaluation and selection application that helps you to make the right decisions about buying, selling, or trading crude oil. These decisions are more critical than ever, as geopolitical considerations and stringent business competition increase the pressure on your ability to achieve or sustain profitability.

Q: What can be expected as a typical logic configuration cost requirement of Asset Manager on a percentage basis of the software cost?
A: The minimum configuration effort needed to see some benefits is one week of configuration. Of course, the more effort put into the configuration of assets with Asset Manager, the greater the long-term return on investment.

Q: How does the ASSAY2 graphical interface work?
A: ASSAY2 accepts data either by a cut-and-paste method, or by Microsoft Excel spreadsheet import. Drag-and-drop features are included for data and property correction. In addition to expanded property capabilities, ASSAY2 also provides you with several other capabilities for added functionality.

Q: What is the ASSAY2 Library Management feature?
A: ASSAY2 includes crude oil Library Management features that allow crude oil libraries to be created, deleted or copied. Another feature imports libraries from other crude assay evaluation applications, from libraries provided by Honeywell, or from properly formatted user spreadsheets. Assay2 also allows crudes to be sorted by categories such as sulfur content, API gravity, geographical origin, or assay data.

Q: How does ASSAY2 break up and blend crude assays?
A: ASSAY2 allows crude assays to be broken up in a manner consistent with individually tailored cut schemes so that the qualities and yields of individual cuts can be evaluated. These qualities can then be used to determine either their singular or comparative values individually, or as blended with other crudes or crude components.

Log In
Search

  Advanced Search
Contact Us
Contact Honeywell Process Solutions