Rashtriya Chemicals & Fertilizers (RCF) of India successfully implemented an Advanced Process Control (APC) upgrade in their 1,500 TPD Ammonia Plant in October 2003. RFC realized a significant reduction in energy usage and steam to carbon ratio.
RCF successfully implemented Honeywell’s Model Predictive Control (MPC) solutions to achieve these key benefits:
Rashtriya Chemicals and Fertilizers Ltd. (RCF), operates a large-scale urea-manufacturing complex with an annual capacity of 1.48 million tons. The urea is manufactured in three trains of equal capacity, and uses ammonia stripping technology supplied by Snamprogetti, Italy. Two trains of ammonia plants, each with a capacity of 1,500 tons per day (TPD), produce the ammonia and carbon dioxide necessary for urea production. Haldor-Topsoe, Denmark supplied the technology for the dual feed of naphtha and natural gas.
Each of the ammonia plants is comprised of the following units:
RCF’s objectives for the APC implementation were:
Honeywell’s Profit Controller (Robust Multivariable Predictive Controller – RMPCT) was used in this project to meet the above objectives. Considering the plant’s constraints, a combination of advanced regulatory control strategies and model-based advanced controls were implemented.
Advanced Regulatory Control (ARC) strategies were implemented by using Application Module (AM) based Control Language (CL) programming. These regulatory level strategies, detailed below, facilitate the functioning of Profit Controller-based strategies.
Profit Controller (RMPCT) strategies - Two RMPCT based applications were implemented to allow independent functioning of the following sections.
The RMPCT application for this section accomplished the following:
Benefit Evaluation: The baseline data was collected and consolidated from three continuous days in November 2003. The post APC implementation data were gathered during March 2004.
To arrive at the accrued benefits from the minimization of specific energy consumption, the two sets of data were compared.
The following table summarizes the comparative study of some critical parameters.
Comparative study of Specific Energy
Honeywell’s Profit Controller solution for RCF is another example of Honeywell’s ability to deliver more than customer’s expectations. The Profit Controller implementation on Ammonia Plant Line-1 at RCF yielded considerable improvements in the stability of plant operations. Furthermore, critical production parameters have been optimized while operating within the plant constraints. Based on the results, RCF decided to proceed with the implementation of the remaining phases and increased the scope of the project. RCF will not be including any guarantees from Honeywell for the subsequent phases.