Honeywell implemented Profit® Loop on the naphtha hydrotreater unit at the Sasol Synfuels facility in Secunda, South Africa to help improve the process control and stability of the unit.
Profit Loop is Honeywell’s patented regulatory control algorithm that functions as a single input/single output (SISO) model predictive controller, specifically designed with the operating simplicity and computational efficiency of a standard PID controller. The technology is based on Honeywell’s patented Robust Multivariable Predictive Control Technology (RMPCT).
With Profit Loop, Sasol was able to:
Sasol is an integrated oil and gas company with substantial chemical interests. The company has developed world-leading technology for the commercial production of synthetic fuels and chemicals from low-grade coal as well as the conversion of natural gas to environment-friendly fuels.
Sasol operates in more than 20 countries and is one of the top five publicly listed companies in South Africa.
Sasol faced the challenge of improving process operations and reducing costs of its naphtha hydrotreater unit. The Synfuels facility operated a cascade loop between the inter-bed temperature transmitter and a hydrogen quench flow controller at its naphtha hydrotreater unit in manual as a result of the inability of standard PID control to handle the process dead time.
Sasol needed an effective method to maintain the temperature as it was a key parameter for the process to run close to the specification on final naphtha nitrogen and phenol content.
Sasol opted for a trial version of Honeywell’s Profit Loop technology to help optimize control of the naphtha hydrotreater unit temperature. The Profit Loop controller uses a simple model of the process to predict the effect of past, present and future control moves on the process variable. Because Profit Loop can anticipate future process behavior, the controller knows exactly how much to move the process in order to meet the desired control objectives. The Profit Loop algorithm capabilities enable the easy replacement and online migration to this technology. The Profit Loop controller configuration is similar to PID, but has a superior algorithm and is easier to tune and maintain than a conventional controller.
The software was installed and commissioned in less than 20 minutes while the plant was running. With migration to the new control technology, the system was equipped to handle difficult process dynamics beyond the scope of a traditional PID controller.
Since Profit Loop can also be applied to virtually any regulatory control problem (temperatures, pressures, flows, discrete analyzers, tank levels, as well as complex dynamics and process delays), the need and expense of loop tuning packages and services is eliminated.
The newly commissioned Profit Loop controller successfully kept the temperature within 1.5 °C of set point yielding a performance better than any control previously attempted on this loop. Sasol was able to reduce the hydrogen consumption on the unit resulting in benefits that covered the cost of purchasing a site-wide license for the software.
Profit Loop is an optional algorithm in Honeywell TDC 3000 and Application Modules and TPS APP Nodes. Profit Loop and Profit Loop Assistant are standard deliverables in the Experion® Process Knowledge System (PKS) as an embedded algorithm in the C300, C200 and ACE/CEE environments.
Profit® Loop and Experion® are registered trademarks of Honeywell International Inc.