“When I think of Honeywell I think of solutions that improve both efficiency and reliability. Honeywell emerged as our preferred vendor of choice because of its direct LNG experience and expertise in that field. Honeywell’s suite of products helped Atlantic LNG both stabilize operations and enhance our production.”
Dawn Beekee, Instrument and Controls Engineer, Atlantic LNG
Atlantic LNG Company of Trinidad and Tobago has four liquefied natural gas (LNG) trains at its facility that have been successfully commissioned and operational. However over the years, multiple modifications were made to the trains to optimize production to fully utilize the basic and advanced regulatory controls available on the DCS. As part of a recent strategic initiative, Atlantic LNG realized the need for more sophisticated technology such as Advanced Process Controls (APC) on its trains. As the first plant to implement an APC system on an LNG plant utilizing the ConocoPhillips Optimized Cascade Process, Atlantic LNG turned to Honeywell’s APC solutions to stabilize operations, increase efficiency, reliability and production.
Atlantic LNG called upon Honeywell to help develop an action plan and implement the APC project resulting in the following benefits on Train 1:
The Atlantic LNG Company of Trinidad and Tobago was formed in July 1995 to develop a liquefied natural gas plant in Point Fortin, Trinidad and Tobago. The venture links together one local company, NGC - National Gas Company of Trinidad and Tobago (Government owned)., and four other companies bringing extensive international experience in the natural gas industry: Amoco Trinidad (LNG) B.V., British Gas Trinidad LNG Ltd., Repsol International Finance B.V. and Cabot Trinidad LNG Limited. Amoco’s shareholding is now held by BP Trinidad (LNG) B.V. and Cabot’s by Suez (Trinidad and Tobago) LNG Ltd.
The plant is located at Point Fortin, on the south-western coast of Trinidad, the larger of the two islands that form the Republic of Trinidad and Tobago. The administrative office is in Port of Spain, the capital city. Trinidad and Tobago are the southernmost islands in the Caribbean Sea.
Atlantic LNG is a liquefied natural gas operating company generating value for shareholders, employees and communities in which they operate. The company is dedicated to the safety of its people and operations and driven to succeed and continually improve, highlight safety of people and operations.
As part of a strategic initiative Atlantic LNG looked to improve its reliability and operational efficiency. Tasked with that challenge, the plant knew it needed to modernize its facility and LNG trains.
In order to upgrade the technology, Atlantic LNG investigated advanced process controls and looked at Train 1 to see if any benefits could be provided by the use of APC. The plant looked to enhance production on two product streams – LNG and NGL – and commenced with a benchmark study on Train 1.
“We wanted to forge new ground with the implementation of a new APC system to help Atlantic LNG optimize its production and needed to select a partner that could take our APC building blocks and arrange them in a way that would help ensure reliable and safe operations and simultaneously increase our production,” said Dawn Beekee, Instrument and Controls Engineer, Atlantic LNG.
As the first plant to implement an APC system on an LNG plant utilizing the ConocoPhillips Optimized Cascade Process, Atlantic LNG conducted a search of partners and invited five to present. Based on the report that came back and the company’s analysis tree, Honeywell emerged as the preferred vendor because of its LNG experience, domain expertise and assigned personnel.
“We turned to Honeywell’s APC solutions to help stabilize operations, increase efficiency and reliability and achieved success in doing so with Train 1 because of the success of our benefits study, economic results and personnel that Honeywell assigned to the project,” continued Beekee.
As part of the process, Atlantic LNG went through a planned workflow approach with Honeywell that included the following:
Atlantic LNG plans to continue to take advantage of Honeywell’s advanced process controls by benchmarking Trains 2 and 3.. Concluded Beekee, “Atlantic LNG learned from the benefits study and with Honeywell’s help of a dedicated project team we were able to meet deadlines, conduct extensive operator training, and establish best demonstrated practices during commission and acceptance phases all with no operational upsets and minimal product losses – ultimately achieving our sought after strategic objective of reliability and operational efficiency.