Implementing Honeywell’s advanced process control software, Oil and Natural Gas Corporation (ONGC), India, increased output by 8655 tonnes per annum from two units. The installed solution includes Profit® Controller, based on Honeywell’s patented Robust Multivariable Predictive Control Technology (RMPCT).
ONGC, a horizontally integrated petroleum company, is India’s most profitable corporation. The company contributes 77 percent of India’s crude oil and 81 percent of natural gas production. The Uran complex of ONGC is a receiving on-shore point for oil and gas from its offshore installations.
The Profit Controller implementation helped ONGC:
In addition, the following installation benefits were realized:
Project goals for the EPRU included:
Project goals for the CFU-II included:
Engineers from ONGC and Honeywell worked together to implement a multivariable predictive controller and inferential property prediction package based on Honeywell’s Profit Controller offering. Profit Controller was implemented on the EPRU and CFU-II. Tuning Profit Controller was easily accomplished with a standard interface, Profit Viewer. All values entered in the advanced process control graphics were checked with the values observed in Profit Viewer.
The ability of the controller to reject various disturbances was easily seen in simulations. Simulations also provided an opportunity for setting the tuning parameters to reasonable initial values.
All the important product qualities were effectively predicted online using Honeywell’s Profit SensorPro technology.
Profit Controller performs the following functions in the EPRU unit:
Profit Controller performs the following functions in the CFU-II unit: