MOL was able to demonstrate a significant return on investment with almost $200K in yearly savings and a huge profit margin increase using Honeywell’s advanced process control solution.
The Hajduszoboszló Gas Plant, belonging to the north production area of the Upstream Division of the MOL Oil & Gas Company, has been running since 1965. During this time there have been continuous improvements to the process and in the control system. The rich gas plant capacity is 2 million m³/year, but the plant is currently running on 1.6 million m³/year capacity. In addition the propane and butane, content of inlet gas also decreased during this time. In response, the plant tries to maintain profitable production through continuous process improvements.
A preliminary benefit study by Honeywell convinced the management of MOL that using advanced process control (APC) can further decrease costs and help maintain profitable production.
With Honeywell’s help, MOL was able to demonstrate the intrinsic value and benefits of Honeywell’s APC solution in less than eight months. Specific benefits included:
A series of successful business transactions transformed MOL from a local Hungarian company into a leading international conglomerate. MOL Group comprises a leading Hungarian chemical company, TVK, the Slovakian oil company, Slovnaft, the Austrian retail and wholesale company, Roth, and a strategic partnership with the Croatian company, INA.
MOL Group is a market leader in each of its core activities in Hungary and Slovakia, including:
As Hungary’s leading oil and gas company, MOL planned to increase the efficiency of its Hajduszoboszlo Gas Processing Plant, where final products produced are propane and butane or a combination mixture and gasoline.
A preliminary benefit study by Honeywell APC engineers convinced MOL management that a successful APC implementation could reduce cost significantly.
After tendering Honeywell’s APC solution, Profit Controller® was chosen as the technology to achieve the economic and operation objectives. Profit Controller provides powerful, easy-to-use APC capabilities through the use of Honeywell’s patented Robust Multivariable Controller Technology (RMPCT).
During the project a number of specific challenges arose and were resolved:
Profit Controller was applied on both Honeywell and third-party control systems. In addition, as Profit Controller manipulates multiple process variables continuously and automatically, it significantly reduces the workload of control room operators, enabling them to spend more time optimizing the process, rather than being involved in the continual adjustment of the process.
The return on investment was crucial in this project. With this successful APC installation, MOL reduced cost and increased profit. The project resulted in a number of key benefits for the customer. Fuel gas flow was reduced, as well as the electricpower consumption of the cooling compressors. A reduction of the column reboiler duties was also observed.