HomeSUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
Article ReprintsEventsNews RoomNewsletterUsers Group SymposiaWebinars
<< Back

Press Release

HONEYWELL EXPANDS AVAILABILITY OF MASTERLOGIC PROGRAMMABLE LOGIC CONTROLLER

Product Features Space-Saving, Pocket-Size Units; Powerful CPUs Process Complex Instructions at High Speeds for Greater Control System Flexibility

PHOENIX, May 5, 2009 – Honeywell (NYSE:HON) today announced it is expanding distribution of its MasterLogic line of high-speed, compact programmable logic controllers (PLCs) to worldwide process manufacturers. MasterLogic brings power and robustness to very high-speed logic, interlock and sequencing applications. MasterLogic is sold, delivered and supported by Honeywell’s expansive global organization.

MasterLogic can be deployed in a stand-alone mode without requiring any human machine interface. It is also an additional controller that can be used with Honeywell’s Experion® Process Knowledge System architecture and is compatible with Honeywell’s portfolio of process control systems, including the recently released Experion LS. As an additional controller tightly integrated to the control system, MasterLogic can help increase operational efficiency by allowing plants to control multiple processes with just one common operator interface.  In addition, this seamless integration can reduce engineering configuration time by approximately 25 to 35 percent over segregated alternatives.  

“Many of our customers see PLCs as cost-effective solutions for very high-speed logic processes, and making those processes are part of the bigger control system allows plants to achieve greater efficiency and greater throughput,” said Tim Sweet, product marketing manager for Honeywell Process Solutions. “The MasterLogic PLC provides the flexibility commonly associated with PLCs and augments it with a global support network and the ability to integrate with the industry’s newest control systems.”

MasterLogic central processing units (CPUs), power supplies, rack sizes and extensive input/output selection are well suited to a large variety of applications. The solution also provides maximum reliability with redundant CPUs, power supplies and networks. Additionally, the compact, pocket-size modules reduce cabinet space requirements.

Engineering the MasterLogic controllers is simple with the flexibility of industry standard IEC-61131-3 programming languages. 

For more information regarding the MasterLogic PLC and other Honeywell solutions that can improve business performance, please visit www.honeywell.com/ps.

Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges.  For more news and information on Honeywell, please visit www.honeywellnow.com.Honeywell Process Solutions is part of Honeywell’s Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Process Solutions, access www.honeywell.com/ps.

This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Experion ® is a registered trademark of Honeywell International Inc.

*All other marks are trademarks of their respective owners.

Log In
Search

  Advanced Search
Contact Us
Contact Honeywell Process Solutions
Contacts

Jake Saylor
602-313-4054
jake.saylor@honeywell.com

Andres Ybarra
952-346-6314
aybarra@webershandwick.com