High-Purity Water System Incorporates ORP Measurement to Minimize Corrosion
PHOENIX, Feb. 9, 2010 – Honeywell (NYSE:HON) today announced it has added oxidation reduction potential (ORP) measurement – a key parameter for minimizing corrosion in power plant equipment such as turbines and piping – to its HPW7000 High-Purity Water Measurement System, which should enable plants to better maintain critical equipment, reduce capital expenses and lower chemical usage.
The HPW7000 is widely used in applications such as boiler feedwater systems in municipal utilities and large industrial plants that produce electricity from on-site power plants. Its specially designed flow chamber and electrode mounting has been used for more than 10 years to simplify installation and calibration while providing highly accurate pH level readings. Adding the ORP electrode gives plant chemists, plant managers, maintenance engineers and safety and reliability engineers a more-accurate picture of oxidation levels in high-purity water systems where the conductivity of the water samples is less than 10 microsiemens per centimeter (uS/cm).
“Reliably measuring ORP levels in these applications has historically been complicated, but it’s a worthwhile investment if plants can use the data to maintain optimal reagent levels in the feedwater and thus reduce corrosion,” said Thomas Griffiths, global product marketing manager. “Incorporating ORP technology into the HPW7000’s easy-to-use design will ultimately minimize maintenance requirements and improve plant uptime.”
For more information regarding the HPW7000, please visit http://hpsweb.honeywell.com/Cultures/en-US/Products/Instrumentation/pH-ORP/HPW7000/default.htm.
Honeywell International (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com. Honeywell Process Solutions is part of Honeywell’s Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Process Solutions, access www.honeywell.com/ps.
This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.