Control System Provides Reliability and Agility in Smaller System, Helps Plants Lower Lifecycle Costs
ORLANDO, Feb. 2, 2009 – Honeywell (NYSE:HON) today introduced the Experionâ LS control system, a new product within Honeywell’s award-winning Experion Process Knowledge System (PKS) line that provides the power and reliability of a distributed control system (DCS) in a small and flexible solution. Experion LS manages all continuous process control applications and optimizes batch and sequence-oriented applications typically found at specialty chemicals, pharmaceutical, food and beverage and consumer goods producers. Scalable from a single PC and controller to multiple stations, Experion LS promotes plant reliability and flexibility while lowering lifecycle costs for smaller manufacturing sites.
Experion LS is uniquely suited for smaller plants because it allows the manufacturer to better respond to market changes while offering robust process and batch control features. Because it requires less engineering effort to configure and is easier to maintain than a PLC or large DCS, Experion LS can help plants save up to $20,000 per year in support per system. The easier configuration also enables faster and more-reliable changeovers, allowing operators to more easily modify batch recipes and increase production.
“Many applications in the Food and Beverage, Specialty Chemical, Pharmaceutical and Life Science industries would benefit from the functionality of a DCS, but the installed base has been limited due to the perceptions of lack of scalability, great complexity and high costs,” said ARC Advisory Group analyst Craig Resnick. “Experion LS appears to address these issues by being designed to be a DCS for the masses, one that can be specified, purchased, installed, and maintained in a scalable fashion by organizations that have not utilized DCS systems in the past. It is especially critical today that manufacturers, processors, and OEMs leverage these technologies in face of their unprecedented pressures to cut costs while simultaneously meeting increased regulations and sustainability objectives.”
“Smaller manufacturing operations tell us they need DCS functionality, such as the system reliability and greater flexibility that PLCs can’t offer, but many leading DCS systems are just too big for their operations,” said Harsh Chitale, vice president of strategy and global marketing, Honeywell Process Solutions. “Experion LS offers the best of both worlds. It provides agility to respond to product mix changes and offers advanced optimization and batch technology usually found in larger DCS systems.”
Experion LS features Honeywell’s S88 compliant and scalable solution for batch automation that can be fully redundant. The system minimizes engineering costs with drag-and-drop configuration, pre-built algorithms, a global database, pre-configured displays and out-of-the-box batch functionality. Operational advantages are gained by being able to make automation configuration changes without stopping production and offering operators a run-time view of control strategy and sequence status, truly redundant unit execution and integrated operator instructions.
“For many years, smaller manufacturers faced a dilemma: They needed to quickly adapt their processes to market changes, but doing so could reduce system reliability and increases lifecycle costs,” said Chitale. “As the creator of the first DCS system, Honeywell has taken its extensive DCS knowledge and designed Experion LS to deliver the agility these manufacturers need to survive in today’s business environment without sacrificing system stability.”
Plants can work through local authorized Honeywell Experion Implementers to provide project implementation and ongoing application support. Honeywell provides training, support and ongoing technical assistance to system integrators to promote project lifecycle success.
For more information about Experion LS and other Honeywell solutions designed to help batch manufacturers improve their process economics and reduce lifecycle costs, please visit www.honeywell.com/ps.
Honeywell International is a $35 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock Exchanges. For additional information, please visit www.honeywell.com. Honeywell Process Solutions is part of Honeywell’s Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Process Solutions, access www.honeywell.com/ps.
This release contains “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management’s assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
Experion® is a registered trademark of Honeywell International Inc.
*All other marks are trademarks of their respective owners.