HOMESUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
Article ReprintsEventsNews RoomNewsletterCustomer Success StoriesUsers Group SymposiaWebinars
<< Back
Press Release
HONEYWELL’S NEWEST EXPERION RELEASE HELPS INDUSTRIAL MANUFACTURERS IMPROVE SAFETY AND RELIABILITY AT PLANTS

Experion Now Includes Embedded Batch and Simulation Capabilities

PHOENIX, June 17, 2008 – Honeywell (NYSE:HON) today released an enhanced version of its Experion® Process Knowledge System (PKS) that allows plant operators to carefully coordinate process control, safety shutdown and fire and gas mitigation steps. In addition to the unique safety instrumented system (SIS) integration, Experion helps improve plant operations through embedded simulation capabilities used for comprehensive operator training and control, display and procedure validation. The system also introduces new integrated batch functionality that can significantly increase production as well as reliability for chemical and life sciences companies.

Experion is Honeywell’s award-winning process automation and control system used to provide operators greater insight into plant operations. The system feeds data from critical plant subsystems directly to operators to help improve decision making in the control room.

“Experion was originally designed to streamline overall operations, and this latest version expands upon that principle by eliminating the need for intermediate devices to relay important information to the nerve center of the plant,” said Harsh Chitale, vice president of strategy and global marketing for Honeywell Process Solutions. “This release is the most efficient system of its kind, and that efficiency translates to safer, more reliable and more profitable plants.”

Through integration with the company’s newest Safety Manager platform, Experion provides crucial safety and fire and gas information, such as pre-shutdown alerts, directly to operators using a common display. This allows Experion to provide operators with plant-wide SIS point data, diagnostics and system information, as well as alarms and events, operator displays and sequence-of-event information. It also reduces overall system and maintenance costs by reducing the amount of installed field sensor equipment.

Experion can also help increase production capacity through the new Experion Batch Manager. The system’s embedded batch functionality allows chemical and life sciences customers to execute batches at the control level, versus using a separate server. This makes the system more reliable, less complex and easier to maintain. One beta customer calculated it would earn several million dollars in additional revenue by moving to a controller-based batch execution system.

Additionally, Experion features embedded integration capability with Honeywell’s UniSim® simulation tool and can be used to train operators on processes before they are implemented in a plant. This approach can help prepare operators for normal and abnormal operations and improves plant reliability by reducing operator errors. Experion’s comprehensive simulation capability also provides significant engineering efficiency by testing control strategies, displays, and procedures before applying them on live processes.

Another key capability of Experion is a unique alarm shelving utility that allows operators to better manage and prioritize alarms on their displays.  This capability is based on several years of collaboration between Honeywell and the Abnormal Situation ManagementÒ consortium in the interest of improving operator effectiveness during abnormal situations that can lead to process upsets.

Experion also provides a reliable interface with third-party subsystems to reduce the overall cost of ownership. The Process Control Data Interface uses universally accepted MODBUS TCP protocol to control devices such as remote terminal units, terminal servers, analyzers and scales.

For more information about Experion and other Honeywell solutions that improve business performance, please visit www.honeywell.com/ps.  

Honeywell International is a $37 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock Exchanges. For additional information, please visit www.honeywell.com. Honeywell Process Solutions is part of Honeywell’s Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Process Solutions, access www.honeywell.com/ps.

This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.
Experion®, UniSim® and Abnormal Situation Management® are registered trademarks of Honeywell International Inc.

*All other marks are trademarks of their respective owners.

Log In
Search

  Advanced Search
Contact Us
Contact Honeywell Process Solutions
Contacts

Jake Saylor
602-313-4054
jake.saylor@honeywell.com

Andres Ybarra
952-346-6314
aybarra@webershandwick.com