HomeSUPPORTINDUSTRIESSOLUTIONSPRODUCTSSERVICESNEWS & EVENTSABOUT USMY ACCOUNT
ChemicalsLife SciencesMarineMining, Metals & MineralsOil & GasPowerPulp, Paper, Printing & CWSRefining
Thermal Power Plants
Co-generation Plants
Combined Cycle Power Plants
Integrated Gasification Combined Cycle (IGCC)
Clean Energy
Reduce Your Carbon Footprint
Upgrade your Control System
Literature
Home > INDUSTRIES > Power > Industrial Power > Simulators > FAQs
 

Simulators: FAQs

Q: What is the difference between low fidelity and high fidelity simulators?

A. Low fidelity simulators offer a lower cost path for conducting simulation exercises. A low fidelity system operates a subset of the processes a high fidelity simulator offers, and does not include testing of the entire system database or other non-combustion control points. A high fidelity system offers a more intensive, true to life simulation, creating an exact replica of the existing plant environment, DCS, and more.

Q: What functions/data points are not included in the base simulator?

A. Burner system simulation functions are not included. The entire system database, data acquisition and other non-combustion control points are usually not simulated.  This may mean that some of the schematic displays will show missing data. A user has the option to add to the base simulation (hardware and software) as desired, to capture the data points needed.

Q: What is required to run the Low Fidelity Utility Plant Simulator?

A. Honeywell recommends that a “stand alone” hardware system be used for the Simulator. The minimum required hardware to run the system includes:

  • Experion server or ACE node – contains the base logic
  • C200 Controller – contains the control system
  • Experion station – the operator window to the system

The minimum software required to run the system includes:

  • Base system software
  • Boiler/Turbine simulation logic – running in the C200 Controller, Experion Server or ACE node

Log In
Search

  Advanced Search
Contact Us
Contact Honeywell Process Solutions